キーワード、オーダーコード、製品コード、またはシリアル番号で検索してください(例:「CM442」や「技術仕様書」)
2 文字以上を入力して検索を開始してください。

The vortex flow measuring principle

For measuring the volume and mass flow of liquids, gases and steam

Video Multiple industries 03.12.2024

This measuring principle is based on the fact that turbulence forms downstream of obstacles in the flow, such as a bridge pier.

Inside each vortex flowmeter, a bluff body is located in the middle of the pipe. As soon as the flow velocity reaches a certain value, vortices form behind this bluff body are detached from the flow and transported downstream. The frequency of vortex shedding is directly proportional to the mean flow velocity and thus to the volume flow.

The detached vortices on both sides of the bluff body generate alternately a local positive or negative pressure that is detected by the capacitive sensor and fed to the electronics as a primary digital, linear signal.

Watch the video to learn how the vortex flow measuring principle works and read more about it here!


Advantages of vortex flowmeters at a glance

  • Universally suitable for measuring liquids, gases and steam
  • Largely unaffected by changes in pressure, density, temperature and viscosity
  • High long-term stability: no zero-point drift, lifetime K-factor
  • No moving parts
  • Little pressure loss
  • Easy installation and commissioning
  • Large turndown of typically 10:1 to 30:1 for gas/steam, or up to 40:1 for liquids
  • Wide temperature range: –200 to +400 °C (–328 to +752 °F) (450 °C / 842 °F on demand)

Transcript Title

The most diverse substances are transported and distributed in piping systems every single day.
They can include solvents and chemicals, oil and gas, coolants in primary industry or steam for energy transmission.
The fluids flowing through pipes often have completely different properties. Consequently, different principles for their measurement are required.
One method is flow measurement based on the vortex principle.
In 16th-century Italy, Leonardo da Vinci observed how vortices form in flowing water. Some 400 years later, Hungarian physicist Theodore von Kármán described the physical laws that govern how these vortices take shape.

Here is how this measurement method works.
Inside each vortex flowmeter, a bluff body is located in the middle of the pipe. This body is a kind of obstruction that disturbs the flow.
Downstream from the bluff body is a mechanical sensor which can register the tiniest pressure differences in the flowing fluid.
If the fluid is not flowing, no vortices form.
As soon as the fluid starts to move and reaches a certain flow rate, vortices gradually appear downstream of the bluff body. These vortices are detached alternately on either side of the bluff body and are carried away by the flowing fluid.

Zones of high or low pressure now appear downstream and thus create a phenomenon that is known as the “Kármán vortex street”.
These differences in pressure exactly match the frequency of the passing vortices and are precisely registered by the mechanical sensor – shown here in slow motion.
This sensor is unique because it is inherently so well balanced that pipe-borne vibrations up to 1 g, pressure surges and temperature shocks have no effect whatsoever on the measurement.
The distance between two consecutive vortices corresponds to a defined volume of fluid; therefore, total flow can be calculated by counting the vortices that pass.

The higher the flow velocity, the higher the measured frequency of vortices.
In some applications, the velocity is too low for perceptible vortices to form. However, the velocity can be increased simply by installing a vortex meter that has a reduced cross section. This modification does not affect measuring accuracy.
Functionality can be enhanced by incorporating optional temperature measurement into the sensor.
A configuration like this – together with a built-in flow computer – can calculate temperature-dependent mass or energy flow. This feature is particularly important in industrial processes involving saturated steam or gases.

In today’s market place, vortex flowmeters from Endress+Hauser are the world’s most robust and reliable with a lifelong calibration factor. They have won several prestigious awards and widespread acclaim.
For all applications, we have the right solution.
Endress+Hauser - your single-source supplier for measurement technology!

Our vortex flowmeters

イベント&トレーニング